* Question
| What is an RS-485 repeater? |
* Answer
| RS-485 repeaters are required in the following cases: more than 32 stations (including repeaters) are connected to the bus or exceed the maximum length allowed by the network segment (related to the transmission rate).RS-485 repeaters are used to connect two segments of the bus in a PROFIBUS network to increase the number of stations. |

COMMENTS