* Question
| What is included in the signal channel section? |
* Answer
| The input of the measured signal channel 1 and the input of the signal channel 2 to be measured are used to access the signal we want to measure, that is, the input of the measured signal.Because it is a dual-trace oscilloscope, there are two channels, which can be connected to two signals at the same time for comparison observation. This is the characteristic of the dual-track oscilloscope.If the peak value of the input signal voltage exceeds this value, it may cause damage to the input channel of the oscilloscope. This requires special attention from the reader. |

COMMENTS