* Question
What is self-inductance?
* Answer
Self-inductance is the property of an electrical circuit—typically a coil or inductor—that causes it to oppose changes in the current flowing through it by generating a voltage (electromotive force, or emf) within the same circuit.
Mathematically:
ε=−L*dI/dt
Where:
ε is the self-induced emf (volts)
L is the self-inductance (henrys)
dI/dt is the rate of change of current with respect to time
Table of Contents
ToggleHow It Works: The Physical Principle
When current flows through a closed loop (such as a coil), it generates a magnetic field. If the current changes over time, the magnetic flux passing through the loop also changes. According to Faraday’s Law of Electromagnetic Induction, this change in magnetic flux induces an emf in the same loop.
This induced voltage:
Opposes the change in the original current (per Lenz’s Law)
Acts as a form of “electrical inertia” that resists rapid current shifts
This entire phenomenon is called self-inductance, and the voltage generated is called the self-induced emf.
Engineering Significance
Self-inductance is a core principle in:
Inductors used in filters, converters, and power supplies
Transformers, where it governs energy storage in primary windings
Circuit protection, where inductance limits current surges
Signal conditioning, particularly in high-speed or RF designs
It explains why circuits with inductors resist sudden current changes—helping to stabilize voltages and suppress noise.
Self-Inductance vs. Mutual Inductance
| Property | Self-Inductance | Mutual Inductance |
| Circuit | Single coil or loop | Two or more coils |
| Cause of emf | Change in own current | Change in current in a nearby coil |
| Application | Inductors, chokes, energy storage | Transformers, coupled coils, wireless charging |
| Symbol | LLL | MMM |
Summary
Self-inductance is the mechanism by which a coil responds to changes in its own current by generating an opposing voltage. It is governed by electromagnetic laws and plays a crucial role in energy conversion, signal integrity, and power management.
Understanding self-inductance is fundamental for working with inductive components and designing reliable analog or power electronics systems.

COMMENTS