* Question
| What is the construction and electrical characteristics of the transformer? |
* Answer
| The transformer is relatively simple in construction and consists mainly of iron cores and turns.The coil, also called the winding, is wound around the core and transmits the alternating magnetic flux generated by the core.The coil has a division of the primary coil and the secondary coil.The primary coil is also called the primary coil or the primary winding; the secondary coil is also called the secondary coil or the secondary winding. |

COMMENTS