* Question
| What is the design and calculation procedure for the capacitor? |
* Answer
| (1) The type of capacitor.It is very important to correctly select the input and output capacitors to ensure the lowest switching noise performance of the input and output.
(2) Input capacitance.It is important that the input capacitor have a low ESR, which can effectively reduce the input current noise.There are two separate requirements for the input capacitor. |

COMMENTS