* Question
| What is the difference between a normal power inductor and a high current inductor? |
* Answer
| The difference between ordinary power inductors and high current inductors has the following characteristics:
1. The flat bottom surface is suitable for surface mounting. 2. Excellent solderability of end face strength. 3. It has the characteristics of high Q value and low impedance. 4. Low magnetic leakage, low straight resistance and high current resistance.It can withstand up to 80A current. 2. High stability. The high current inductor adopts fully enclosed magnetic shielding structure, which has good sealing and high stability. 3. Wide application range. High current inductance has superior weather resistance.For computer motherboards, microcontrollers, graphics cards, etc. These long-time devices. And ordinary power inductors can only be used as DC-DCDetermine the performance of the motherboard. |

COMMENTS