* Question
What is the electrochemical cell?
* Answer
An electrochemical cell is a device that converts chemical energy into electrical energy or vice versa through a redox (reduction-oxidation) reaction. It typically consists of two electrodes (an anode and a cathode) immersed in an electrolyte, which allows the flow of ions. The electrochemical reaction that occurs at the electrodes generates an electrical current, which can be used to power devices or stored for later use.
Table of Contents
ToggleComponents of an Electrochemical Cell:
Electrodes:
Anode: The electrode where oxidation occurs (loss of electrons).
Cathode: The electrode where reduction occurs (gain of electrons).
Electrolyte: A conductive solution or paste that allows ions to move between the electrodes, completing the electrical circuit. It can be liquid, gel, or solid.
External Circuit: A conductor (usually a wire) that connects the two electrodes, allowing electrons to flow from the anode to the cathode, creating an electric current.
Salt Bridge or Porous Partition: In some electrochemical cells, a salt bridge or a porous barrier separates the two electrolyte solutions to prevent mixing while allowing ion flow between the compartments.
Types of Electrochemical Cells:
Galvanic Cells (Voltaic Cells): These cells generate electrical energy from spontaneous chemical reactions. They are commonly used in batteries. For example, in a common zinc-carbon battery, zinc serves as the anode, and carbon serves as the cathode.
Electrolytic Cells: These cells use electrical energy to drive non-spontaneous chemical reactions, such as electroplating or the electrolysis of water to produce hydrogen and oxygen. An external power source is required to drive the reaction.
Example: The Daniell Cell
A typical example of an electrochemical cell is the Daniell cell, which consists of a copper electrode in a copper sulfate solution and a zinc electrode in a zinc sulfate solution. In this setup:
Anode (Zinc): Zinc undergoes oxidation, releasing electrons.
Cathode (Copper): Copper ions gain electrons and are reduced to solid copper.
Electrolytes: Zinc sulfate (ZnSO₄) and copper sulfate (CuSO₄) act as the electrolyte solutions.
The flow of electrons through the external circuit from the zinc electrode (anode) to the copper electrode (cathode) generates electrical energy.
Applications of Electrochemical Cells:
Batteries: Commonly used in portable devices (like smartphones and laptops).
Fuel Cells: Convert chemical energy from fuels (e.g., hydrogen) into electricity, with applications in clean energy technologies, including electric vehicles.
Electroplating and Electrolysis: Used for coating objects with a layer of metal and for chemical production processes (e.g., chlorine production).
In summary, electrochemical cells are essential components in energy storage and conversion technologies, with applications spanning from energy generation to chemical manufacturing.

COMMENTS