* Question
What is the group low power function? |
* Answer
When the A/D converter is not used, the ladder Resistors of the A/D converter is disconnected from the reference voltage input pin (vREF) through the VCUT bit of the ADCON1 register, and the current does not flow from the VREF pin to the ladder Resistors, thereby reducing the power.Consumption.It should be noted that this function does not affect the Vref of the D/A converter because they are irrelevant. |
COMMENTS