* Question
What Is the Main Function of the Event Trigger (ET) Module?
* Answer
The main role of the Event Trigger (ET) module is to monitor predefined conditions or signals and initiate specific system actions when those conditions are met. It acts as a bridge between event detection and system response, enabling timely, condition-based control and processing.
1. Event Detection and Monitoring
The ET module continuously monitors internal or external signals, such as:
- Sensor outputs
- Status flags or system variables
- Timing thresholds or interrupt signals
When a predefined event occurs, the ET module identifies it accurately and reliably.
2. Triggering System Actions
Once an event is detected, the ET module generates trigger signals to activate corresponding system responses. These responses may include:
- Starting or stopping a control process
- Initiating data acquisition or logging
- Generating interrupts or control flags
This mechanism ensures that system actions are executed precisely when required.
3. Improving Real-Time Responsiveness
By responding directly to events rather than relying on continuous polling, the ET module helps reduce system latency.
This event-driven operation is especially important in real-time systems, where fast and deterministic response is critical.
4. Reducing CPU Load and System Overhead
The ET module offloads event detection tasks from the main processor.
Instead of repeatedly checking conditions in software, the system reacts only when an event occurs, improving processing efficiency and overall system performance.
5. Enhancing System Reliability and Determinism
Because events are handled through well-defined trigger mechanisms, the ET module contributes to predictable system behavior.
This is essential in control, automation, and embedded applications where timing accuracy and stability are required.
Summary
The Event Trigger (ET) module plays a key role in detecting predefined events and initiating corresponding system actions in a timely and efficient manner. By enabling event-driven control, it improves real-time responsiveness, reduces processing overhead, and enhances overall system reliability.

COMMENTS