• Home
  • QUESTIONS & ANSWERS
  • RF/IF and RFID
  • What Is the Purpose of the OC Squat Test in a Pull-Out Test?

    * Question

    What Is the Purpose of the OC Squat Test in a Pull-Out Test?

    * Answer

    The OC squat test (Open-Circuit Squat Test) is used during a pull-out test to monitor electrical continuity while mechanical force is applied.
    Its main purpose is to determine whether an electrical connection fails electrically before it fails mechanically.

    In other words, the OC squat test checks if the circuit opens (loses contact) while the conductor or terminal is being pulled.

    1. What the Pull-Out Test Evaluates

    A pull-out test applies a controlled tensile force to a wire, terminal, or connector to measure:

    • Mechanical retention strength
    • Crimp or joint reliability
    • Resistance to separation under load

    Traditionally, this test focuses on mechanical failure, such as wire breakage or terminal pull-out.

    2. What the OC Squat Test Adds

    The OC squat test adds electrical monitoring to the pull-out process.

    During the test:

    • A small electrical signal passes through the connection
    • The system continuously checks for open-circuit conditions

    If the electrical path opens before physical separation occurs, it indicates a hidden reliability issue.

    3. Why Electrical Monitoring Is Important

    Without the OC squat test:

    • A connection may appear mechanically strong
    • But may already have intermittent or unstable electrical contact

    The OC squat test helps detect:

    • Poor crimp quality
    • Internal conductor damage
    • Micro-movements causing contact loss
    • Weak solder or weld joints

    This ensures the connection is electrically reliable, not just mechanically intact.

    4. Typical Application Scenarios

    The OC squat test is commonly used in:

    • Automotive wiring harness testing
    • Connector and terminal qualification
    • Aerospace and industrial cable assemblies
    • Quality control for crimped or welded joints

    In these applications, electrical continuity under mechanical stress is critical for system safety and reliability.

    Engineering Insight

    A good connection should:

    • Maintain electrical continuity
    • Up to and including mechanical failure

    If the circuit opens early during a pull-out test, it indicates the connection may fail in real-world vibration or load conditions, even if it passes basic strength requirements.

    Conclusion

    The purpose of the OC squat test in a pull-out test is to detect open-circuit conditions while mechanical force is applied.
    It verifies that an electrical connection remains stable under stress and does not lose continuity before mechanical failure occurs, providing a more complete assessment of connection quality and reliability.

    COMMENTS

    WORDPRESS: 0
    DISQUS: 0