* Question
| What is the safe operating procedure for electrical equipment commissioning? |
* Answer
| (1) Before the test, the power switch should be disconnected and the voltage regulator should be set to zero position; if a problem occurs during the test or the test is over, the regulator should be immediately returned to the zero position and the power switch should be opened; if it occurs during the testIf the problem is solved, the test can be continued.
4) High-voltage test and more complicated circuit test. After connecting the line, it should be reviewed by the person in charge of the work. After the error, the test can be carried out, and an empty test should be carried out before accessing the test object. (5) After the high voltage test is completed, the equipment should be discharged. 7) When conducting the adjustment test, the test object must be separated from other equipment and kept at a certain safe distance, or insulated with insulation; when the fence cannot be installed or the warning sign is hoisted, a guard should be set up. |

COMMENTS