* Question
What is the test principle of COS functional test?
* Answer
The test principle of a COS (Chip Operating System) functional test revolves around verifying that the smart card or secure chip’s embedded operating system (COS) performs correctly according to its functional specifications. This involves testing how the COS handles command execution, file management, security mechanisms, and data integrity through standardized communication protocols (usually APDU commands).
Table of Contents
ToggleWhat is COS?
COS (Chip Operating System) is the firmware that runs on smart cards, SIM cards, secure elements (SE), and other embedded security chips. It manages:
File systems (EF, DF, MF)
Cryptographic operations
User authentication
Communication protocols (ISO 7816, GlobalPlatform)
Test Principle of COS Functional Testing
1. Command-Response Validation (APDU Testing)
Principle: Send specific Application Protocol Data Units (APDUs) to the card and verify the correctness of responses.
APDU Command: The host sends a request (e.g., SELECT FILE, READ BINARY).
APDU Response: The card replies with data and a status word (e.g., 9000 = success).
Test checks whether:
The command is correctly processed.
The response content and status code are valid.
2. File System Operation Testing
Principle: Verify that COS properly manages its internal file system.
Tests include:
File selection (MF, DF, EF)
File creation, deletion
Reading and writing to files
Access condition enforcement (read/write protections)
3. Security Mechanism Verification
Principle: Ensure the COS enforces security rules like:
PIN/PUK authentication
Key-based authentication
Secure messaging (MAC/encryption)
Access rights and role-based controls
Also involves:
Testing failed login attempts
PIN retry counters
Session timeout behavior
4. Crypto Functionality Test
Principle: If the COS includes cryptographic features (e.g., AES, DES, RSA), functional tests validate:
Key generation
Digital signature and verification
Encryption and decryption
Hashing operations
Outputs are compared against known-good cryptographic values.
5. Protocol Compliance and Error Handling
Principle: Test whether the COS:
Adheres to standards (ISO 7816, GlobalPlatform, ISO/IEC 14443, etc.)
Responds correctly to invalid or malformed APDUs
Handles protocol-level exceptions gracefully
Summary Table
Test Area | Principle |
APDU command/response | Verifies logical correctness of functional command execution |
File system | Tests file navigation, read/write, creation, and access rules |
Security/authentication | Validates enforcement of PIN, keys, and secure sessions |
Crypto features | Ensures correctness of cryptographic operations |
Error handling | Tests abnormal scenarios and COS resilience to invalid input |
Tools Commonly Used
Card reader with ISO 7816 interface
APDU script engines (e.g., GlobalPlatformPro, JCIDE)
COS Test Suites developed per project specifications
Simulators or emulators for pre-silicon testing

COMMENTS