* Question
| What should I pay attention to when using Altera’s configuration chip? |
* Answer
| Make sure the configuration chip is programmed properly.The GM pins cannot be left floating and they should be pulled to a fixed level to select the page on which the profile is located.If using an enhanced configuration device, the external Flash interface pins should be left floating or placed in a high-impedance state while in System Programming and configuring the FPGA. |

COMMENTS