• Home
  • QUESTIONS & ANSWERS
  • Integrated Circuits (ICs)
  • Which feedback modes does the Cyclone III PLL support?

    * Question

    Which feedback modes does the Cyclone III PLL support?

    * Answer

    Cyclone III devices provide several PLL feedback/compensation modes to support different timing and clock-distribution scenarios. The main feedback modes are:

    1. Internal Feedback Mode (Normal Mode)

    • The PLL uses an internal feedback path.
    • The output clock is phase-aligned with the reference clock inside the PLL.
    • Simplest configuration; suitable for most general-purpose applications.

    2. Zero-Delay Buffer (ZDB) / External Feedback Mode

    • The feedback is taken externallyfrom a PLL output pin and routed back to the PLL’s feedback input.
    • Eliminates clock tree delay so the output clock edge aligns with the input clock edge at the device boundary.
    • Commonly used for driving external devices that require tight phase alignment.

    3. Source-Synchronous Compensation Mode

    • The PLL compensates for input or output delaysin source-synchronous interfaces.
    • Used when capturing data using an incoming clock or forwarding a clock with data.
    • Supports DDR, high-speed I/O, and other timing-critical interfaces.

    4. No Compensation Mode

    • The PLL does notperform delay compensation.
    • Used for applications where only frequency synthesis is required, not phase alignment.

    Summary

    Cyclone III PLLs support the following feedback/compensation modes:

    • Internal Feedback (Normal)
    • External Feedback / Zero-Delay Buffer (ZDB)
    • Source-Synchronous Compensation
    • No Compensation

    These modes allow designers to meet a wide range of timing, synchronization, and interface requirements in FPGA-based systems.

    COMMENTS

    WORDPRESS: 0
    DISQUS: 0