• Home
  • QUESTIONS & ANSWERS
  • Integrated Circuits (ICs)
  • Which Signals on the Spartan-3E FPGA Experiment Board Are Directly Driven Through Resistors?

    * Question

    Which Signals on the Spartan-3E FPGA Experiment Board Are Directly Driven Through Resistors?

    * Answer

    On the Spartan-3E FPGA Experiment Board (commonly based on Xilinx Spartan-3E devices), several output signals are directly driven by FPGA I/O pins through series or current-limiting resistors.
    These resistors are used to limit current, protect FPGA I/O pins, and ensure reliable visual or electrical operation.

    The signals most commonly driven through resistors are described below.

    1. User LEDs

    Primary Resistor-Driven Signals

    The on-board user LEDs are the most typical signals driven through resistors.

    • Each LED is connected to an FPGA GPIO pin
    • A series current-limiting resistor(typically 220 Ω–470 Ω) is placed between the FPGA pin and the LED

    Purpose

    • Prevents excessive current from damaging the FPGA I/O
    • Ensures consistent LED brightness
    • Allows direct FPGA control without external components

    These LEDs are widely used for:

    • Logic verification
    • Debug output
    • Status indication

    2. Seven-Segment Display Segments

    Many Spartan-3E experiment boards include one or more seven-segment LED displays.

    Resistor Usage

    • Each segment (a–g, and sometimes the decimal point) is driven by an FPGA pin
    • Individual resistorsare used for each segment line

    Why Resistors Are Required

    • LED segments are current-driven devices
    • Direct connection without resistors could exceed FPGA I/O current limits

    This allows the FPGA to directly control numeric or hexadecimal display output.

    3. Discrete Indicator LEDs (Status or Power Indicators)

    Some boards include additional status LEDs (e.g., configuration done, user-defined indicators).

    • These LEDs are also FPGA-controlled
    • Each is connected via a current-limiting resistor

    4. Why Only These Signals Are Driven Through Resistors

    Not all FPGA signals require resistors.

    Resistor-Driven Signals

    • LEDs
    • Seven-segment displays
    • Other current-sensitive visual indicators

    Non-Resistor Signals

    • Push buttons (use pull-up or pull-down resistors instead)
    • Slide switches
    • External connectors (VGA, SRAM, Flash, PMODs)

    These typically rely on logic-level signaling, not current-driven loads.

    Engineering Insight

    FPGA I/O pins are designed for logic signaling, not for driving loads directly.
    By placing resistors in series with LEDs and display segments, the Spartan-3E board:

    • Protects FPGA output drivers
    • Ensures long-term reliability
    • Simplifies beginner and educational experiments

    This design practice is standard across FPGA development boards from Xilinx, Intel (Altera), and Lattice.

    Conclusion

    On the Spartan-3E FPGA experiment board, the signals directly driven through resistors are primarily:

    • User LEDs
    • Seven-segment display segments
    • Other FPGA-controlled indicator LEDs

    The resistors serve as current-limiting and protection components, allowing safe and direct FPGA control of visual output devices.

    COMMENTS

    WORDPRESS: 0
    DISQUS: 0