• Home
  • Electronics Expo
  • Quality Articles
  • CR2450 Battery: powering up the modern world

    When it comes to the world of coin cell batteries, the CR2450 battery isn’t just another face in the crowd. This power-packed component is essential in various applications, from everyday devices to specialized equipment.

    Unveiling the power of the CR2450

    The CR2450 coin cell battery stands out as a powerhouse in its category, boasting an impressive diameter of 24 millimeters, making it one of the giants among coin batteries. This non-rechargeable 3V lithium cell is a top choice in a wide array of electronic applications, including various car key fobs. Its generous size enables the CR2450 to store more energy than most of its rivals, making it ideal for devices with higher power demands.

    While the 2430 already impresses with its size and capacity, the CR2450 goes a step further with its added thickness and energy reserves. For those searching for of even more power, there’s the chunkier variant, the CR2477. Yet, the 2450 is just the tip of the iceberg; a vast range of lithium coin cell batteries awaits to cater to diverse needs.

    How CR2450 stands out

    Among the sea of coin cells, such as CR2032, CR1616 battery, and CR1620 battery, the CR2450 is distinguishable. Let’s see why:

    • Voltage: The 2450 battery delivers a consistent 3 volts. This ensures that devices don’t just run; they run optimally.
    • Size and weight: Bigger than the 2032 and 1616 battery, but offering more power per gram.
    • Durability: These batteries are designed for longevity. They don’t give up easily!

    Wide selection of CR2450 batteries from leading brands

    Explore our diverse range of CR2450 batteries, featuring top-tier brands such as Panasonic, Renata, and Maxell. These renowned names are synonymous with superior battery quality and longevity. Given its lithium content, the CR2450 battery has an impressively long shelf life, making it wise to keep a few in stock. This ensures you always have the right coin cell battery at hand, eliminating any last-minute rushes. Regardless of your brand preference, rest assured of compatibility.

    CR2450 battery codes

    While the standard code for the CR2450 battery is, indeed, CR2450, it’s not uncommon to find alternative codes inscribed on the battery. This discrepancy arises as different brands employ unique codings, usually followed by the voltage, such as 3V or 3 volts. If your old battery showcases reference numbers like 2450, ECR2450, KCR2450, 5029LC, or CR 2450, don’t fret; they’re essentially the same battery, simply under a different label.

    However, there’s an exception to be aware of: the BR2450 code. This denotes a different chemical composition, specifically a low drain lithium carbon monofluoride battery, designed to deliver consistent voltage. Should you require this variant, be sure to specifically seek out BR2450, as the regular CR2450 won’t suffice in such instances.

    Comparing the Cousins: CR2450 vs others

    While CR2450 is in the limelight, let’s not forget its counterparts.

    • CR2032: Often found in smaller devices, like watches or remotes.
    • CR1616 Battery: Perfect for thinner devices, thanks to its lean profile.
    • CR1620 Battery: Sits between the CR1616 and CR2450 in terms of capacity and size.

    Each of these has its merits, but if you’re looking for a combination of durability and capacity, CR2450 is your winner.

    Applications that rely on CR2450

    You might be surprised to discover where you can find CR2450 batteries. From the digital thermometer that ensures your safety to the garage remote that provides convenience, its presence is felt in many aspects of our daily lives. Also, they are prominent in portable electronic devices where a compact, yet potent power source is a necessity. So, the next time your device powers up swiftly, take a moment to appreciate the unsung hero, the CR2450.

    Storing CR2450 batteries

    CR2450 batteries are celebrated for their prolonged shelf life, allowing for extended storage before use. Many of these batteries boast a lifespan of up to 8 years. Yet, it remains crucial to double-check the expiration date on the packaging. Store these petite power packs in a dry spot at room temperature. Additionally, it’s vital to retain the original packaging. Our lithium coin cells come in ‘child safety’ packs, necessitating scissors for removal. While it may seem cumbersome, this design choice mitigates accidental ingestion risks for toddlers. If you opt to store batteries sans packaging, ensure they’re placed high out of children’s reach.

    Why WIN SOURCE recommends CR2450

    At WIN SOURCE, we’re not just about selling components. We’re about quality, reliability, and ensuring our customers have access to the best. When it comes to coin cell batteries, we’ve seen the incredible value that CR2450 brings to the table. From its extended shelf life to its consistent voltage delivery, it’s clear why this battery is in high demand. We stand by its performance and durability. Whether you’re a tech enthusiast or a professional seeking a reliable component, CR2450 won’t disappoint.

    Convinced about the prowess of the CR2450 battery? Or perhaps you’re curious about its cousins, the CR2032, CR 1616 battery, or CR 1620 battery? Whatever your needs, WIN SOURCE has got you covered. Visit our product store to explore the best in electronic components.

    © 2025 Win Source Electronics. All rights reserved. This content is protected by copyright and may not be reproduced, distributed, transmitted, cached or otherwise used, except with the prior written permission of Win Source Electronics.