• Home
  • Electronics Expo
  • Quality Articles
  • What Is the Difference Between −4.5 V and −10 V Gate Drive for the FDS6681Z?

    In MOSFET selection, gate-to-source voltage directly affects on-resistance, which in turn influences power loss and thermal performance. The FDS6681Z is a −30 V P-channel PowerTrench MOSFET with a maximum RDS(on) of 4.6 mΩ at VGS = −10 V and 6.5 mΩ at VGS = −4.5 V. Understanding the difference between these two operating points helps engineers evaluate how the device will perform under actual gate-drive conditions in power management and load-switching applications.

    1. −4.5 V and −10 V Gate Drive Provide Different Conduction Performance

    For a P-channel MOSFET, the device turns on when the gate voltage is sufficiently lower than the source voltage, creating a negative VGS. Within the specified operating range, a more negative VGS generally enhances the channel further and reduces RDS(on).

    The FDS6681Z datasheet specifies two operating points. At VGS = −10 V, the maximum RDS(on) is 4.6 mΩ, while at VGS = −4.5 V, the maximum value is 6.5 mΩ. Both are manufacturer-specified test conditions. The difference should not be interpreted simply as “fully on” versus “not fully on.”

    For systems with limited gate-drive amplitude, the −4.5 V condition still provides a clearly specified design point. If the load current is higher and the system can provide a VGS close to −10 V, the lower RDS(on) can help reduce conduction loss and voltage drop. In practical device selection, the RDS(on) value should therefore be chosen according to the actual gate-to-source voltage rather than by referring only to the lowest value shown in the datasheet.

    2. Differences in RDS(on) Affect Power Loss and Thermal Design

    When a MOSFET is operating in steady-state conduction, its conduction loss can be approximated as:

    Pcond ≈ I² × RDS(on)

    Using a 10 A load current as an example and calculating with the maximum datasheet RDS(on), the conduction loss is approximately 0.46 W at a −10 V gate drive and about 0.65 W at −4.5 V. As load current increases, the effect of the RDS(on) difference on power dissipation and temperature rise becomes more significant.

    This is why gate-drive conditions should not be evaluated independently from the system load. For low- to moderate-current applications, either operating point may meet the design requirements. In systems with sustained higher current, battery power, or limited PCB thermal capacity, reducing conduction loss may provide greater system-level benefit.

    Temperature must also be included in the calculation. MOSFET RDS(on) changes with junction temperature, so power loss under actual operating conditions should not be estimated using only values near 25°C. PCB copper area, ambient temperature, duty cycle, and nearby heat sources also influence the final junction temperature. In this sense, VGS defines the starting point for the electrical assessment, while the thermal environment determines how that parameter translates into real system performance.

    3. Gate-Drive Conditions Should Match the Actual Power Architecture

    If the system can reliably provide a VGS close to −10 V and the load current is relatively high, this drive condition allows the FDS6681Z to make better use of its low on-resistance. In power-path control, load switching, and battery-powered systems, this can help reduce both MOSFET voltage drop and conduction loss.

    For systems with a lower gate-drive amplitude, −4.5 V is also a valid operating condition with a specified RDS(on) value. One important point is that VGS refers to the voltage difference between the gate and source. It is not simply the output voltage of the MCU or controller. In a high-side P-channel switching configuration, for example, the source voltage follows the supply rail, so the actual gate-to-source voltage must be evaluated from the real node voltages in the circuit.

    The FDS6681Z has an absolute maximum gate-to-source voltage rating of ±25 V. In designs with a wide battery-voltage range or possible supply transients, the maximum VGS condition should also be checked. The objective is to keep the gate drive within the device rating rather than simply applying a larger negative VGS to obtain a lower RDS(on).

    The FDS6681Z provides clearly specified on-resistance values at both −4.5 V and −10 V gate drive. The key design consideration is not which voltage is inherently “better,” but how the actual VGS, load current, power-loss budget, and thermal conditions fit together. For engineering evaluation, using the RDS(on) value that corresponds to the real drive condition is more meaningful than comparing only the lowest on-resistance figure. WIN SOURCE provides FDS6681Z-related component and supply information, as well as support for BOM evaluation and component sourcing. Final design decisions should still be verified against the latest onsemi datasheet and the actual operating conditions of the system.

    © 2026 Win Source Electronics. All rights reserved. This content is protected by copyright and may not be reproduced, distributed, transmitted, cached or otherwise used, except with the prior written permission of Win Source Electronics.