Building automotive products means making a commitment to long-term support. A vehicle platform typically requires 10-15 years of supply support, while many semiconductors may remain commercially available for only 3-5 years. More importantly, these timelines are moving in opposite directions: chip commercial lifecycles are shortening, while vehicle service and maintenance requirements are extending.
At the same time, lead times for automotive MCUs, power devices and MLCCs are becoming increasingly extended. But for automotive procurement teams, the bigger challenge is often not price increases. It is end-of-life.
Why EOL Is Becoming Harder to Manage
On the surface, an EOL (end-of-life) notice is simply a notification. The real problem is timing. The window between a device being classified as NRND (Not Recommended for New Designs) and the Last Time Buy (LTB) can be only a few months. For example, Renesas issued EOL notices covering several SRAM products, leaving customers roughly six months for Last Time Buy purchases – far shorter than the production life these devices may need to support.
The transition itself cannot happen overnight. Replacing an automotive-grade component may require AEC-Q qualification and system-level validation, often taking several months. By the time an EOL notice arrives, there may already be too little time to complete the change safely.
Three Things Procurement Teams Need to Address
Short EOL windows require earlier action.
EOL notices for automotive part numbers may arrive during the later stages of mass production, when the available response window is already limited. Treating EOL as something to plan for – rather than something to handle after receiving a notice – is the first major shift in procurement practice.
Total lifecycle demand needs to be calculated.
For a platform that must be supported for 10-15 years, procurement teams need to estimate remaining demand before an EOL event, then compare it with available inventory and the Last Time Buy window. Knowing exactly how much is missing, and when the gap will occur, is more useful than simply knowing that a part is “out of stock.”
Legacy part numbers still need a long-term supply path.
Some discontinued components remain necessary for years after production ends. The ability to consistently source verified legacy inventory can directly determine whether a production line can continue operating after the original supplier has discontinued the part.
What Procurement Can Do in Advance
- Include EOL signals in routine BOM reviews.
Track the NRND, PCN (Product Change Notification) and EOL status of every relevant part number, and establish internal warning thresholds. For example, an NRND status can automatically trigger a review.
- Build a demand model for long-lifecycle platforms.
Estimate total demand for each critical part based on the platform’s remaining production volume, and regularly reconcile it against inventory, open orders and the Last Time Buy window. This turns EOL exposure into a measurable supply gap.
- Complete alternate-source validation before EOL.
For automotive part numbers with single-source risk, start AEC-Q alternative qualification early. Because qualification takes time, waiting for the EOL notice is often too late.
- Establish stable supply channels for legacy parts.
For parts that will still be required after discontinuation, identify reliable long-term sources in advance and secure a verified inventory position rather than searching for supply only after the part becomes obsolete.
When the Car Outlives the Chip
For automotive procurement teams, the real challenge is no longer just that components are expensive or lead times are long. It is that the product timeline is gradually falling out of sync with the component timeline.
Vehicle platforms need to be planned in terms of decades, while component supply risks can change within months.
That is pushing automotive component procurement away from a simple “buy what is missing” approach toward continuous management of supply availability, product lifecycle, alternatives and long-term inventory.
Through its global supplier network, WIN SOURCE can assist in sourcing automotive-grade and legacy components based on specific requirements and provide potential replacement options for reference, helping procurement teams explore possible alternatives for components approaching EOL.
©2026 Win Source Electronics. All rights reserved. This content is protected by copyright and may not be reproduced, distributed, transmitted, cached or otherwise used, except with the prior written permission of Win Source Electronics.