• Home
  • Q&A
  • RF/IF and RFID
  • What Are the Common Command and Response Formats, and How Are VICC States and State Transitions Defined?

    * Question

    What Are the Common Command and Response Formats, and How Are VICC States and State Transitions Defined?

    * Answer

    What Are VICC Commands and Responses?

    In RFID systems, a VICC (Vicinity Integrated Circuit Card) communicates with a reader through a series of commands and responses. The reader sends a command to request information or trigger an action, and the VICC processes the request and returns a response containing the requested data or status information.

    The command and response structure defines how devices exchange information and ensures reliable communication between the reader and the VICC.

    VICC communication formats are commonly defined by standards such as ISO/IEC 15693, which specifies the air interface, command structure, data exchange procedures, and card behavior for vicinity cards.

    What Are the Common VICC Command Formats?

    A typical VICC command consists of several fields that provide instructions and control information for the card.

    Common command fields include:

    • Flags– Define communication options, such as addressing mode, data rate, and additional requirements.
    • Command code– Specifies the operation requested by the reader.
    • Parameters– Provides additional information required to execute the command.
    • Data field– Contains optional information, such as data to be written to the VICC.
    • Error detection information– Ensures communication reliability.

    Depending on the command type, a request may be used for operations such as:

    • Reading memory contents
    • Writing data to memory
    • Locking memory blocks
    • Retrieving identification information
    • Managing specific VICC functions

    The exact command format depends on the communication protocol and the functions supported by the VICC.

    What Are the Common VICC Response Formats?

    After receiving and processing a command, the VICC sends a response back to the reader.

    A typical response may include:

    • Response flags– Indicate the status of the response.
    • Error information– Shows whether the command was successfully executed.
    • Returned data– Contains requested information, such as identification data or memory contents.

    If the command is executed successfully, the VICC returns the requested information. If an error occurs, the response may include an error code indicating the reason for failure.

    A well-defined response format allows the reader to determine whether the operation was completed correctly and what action should be taken next.

    What Are VICC States?

    A VICC does not continuously perform the same operation. Instead, it operates through different states depending on the communication process and commands received.

    Typical VICC states may include:

    Ready State

    In the ready state, the VICC is powered by the reader’s RF field and is waiting for commands.

    Quiet State

    A VICC enters the quiet state when it has been identified but should temporarily stop responding to certain commands. This helps the reader communicate with other cards in the field without interference.

    Selected State

    In the selected state, a specific VICC has been addressed by the reader and can respond to commands intended for that card.

    Other Operational States

    Depending on the protocol implementation, additional states may exist to support specific functions, memory operations, or communication procedures.

    How Do VICC State Transitions Work?

    VICC state transitions occur when the card receives specific commands or when communication conditions change.

    For example:

    • A newly detected VICC may enter the ready stateafter receiving power from the RF field.
    • After an identification process, the reader may move a specific VICC into the selected state.
    • A VICC may enter the quiet stateafter receiving a command that temporarily disables normal responses.
    • Additional commands may return the VICC to another operational state.

    The state transition mechanism ensures that multiple VICCs can operate in the same RF environment while avoiding communication conflicts.

    Why Are Command Formats and State Transitions Important?

    Understanding VICC command formats and state transitions is important for designing reliable RFID communication systems.

    Proper command handling helps ensure:

    • Accurate data exchange between readers and cards
    • Efficient multi-card identification
    • Reliable memory access operations
    • Compatibility between different RFID devices

    For engineers working with RFID readers, tags, or embedded systems, understanding these communication structures helps simplify system design and troubleshooting.

    Summary

    VICC command and response formats define how RFID readers and vicinity cards exchange information. Commands typically contain control fields, operation codes, parameters, and optional data, while responses provide execution status and requested information.

    VICC states and state transitions define how a card behaves during communication, allowing multiple devices to communicate efficiently within the same RF environment.

    A clear understanding of these mechanisms is essential for developing and integrating RFID systems based on standards such as ISO/IEC 15693.