• Home
  • QUESTIONS & ANSWERS
  • Others
  • What are the basic transmission components of PWE3?

    * Question

    What are the basic transmission components of PWE3?

    * Answer

    PWE3 (Pseudowire Emulation Edge-to-Edge) defines a way to transport packet-based services (like Ethernet) over existing transport networks such as SDH/SONET, ATM, or MPLS. Its basic transmission components are designed to emulate a point-to-point service across a packet-switched network. The key components include:

    1. Ingress and Egress Attachment Circuits (ACs):
    • The attachment circuits connect the customer service interface (like Ethernet) to the PWE3 network.
    • Ingress ACmaps the incoming service into the pseudowire.
    • Egress ACmaps the pseudowire back to the customer-facing interface.
      1. Pseudowire (PW):
    • The core element that emulates the native service over the packet-switched network.
    • Carries the encapsulated payload (e.g., Ethernet frames, ATM cells) across the network.
    • Includes PW headersthat maintain sequence, timing, and control information.
      1. PW Labeling / MPLS or L2TPv3 Tunnels:
    • Labels or tunnel identifiers are used to route the pseudowire through the transport network.
    • For MPLS networks, MPLS labelsidentify the specific PW.
    • For IP-based transport, L2TPv3 or GRE tunnelsmay be used.
      1. Transport Network (T-NET):
    • The underlying network that carries the encapsulated pseudowire, which could be MPLS, IP, or ATM networks.
    • Provides connectivity between PWE3 edge devices.
      1. Control and Management Components:
    • Mechanisms to establish, maintain, and monitor the pseudowire.
    • Include LDP (Label Distribution Protocol)for MPLS-based PWs or other signaling protocols.
      1. Encapsulation and Sequencing:
    • Encapsulation methods wrap customer frames with headers needed for transport.
    • Sequence numbers ensure in-order delivery and detect lost packets.

    In summary, the basic transmission components of PWE3 are Attachment Circuits (ACs), Pseudowires (PWs), label/tunnel identifiers, the transport network, control signaling, and encapsulation/sequencing mechanisms. These components together provide a transparent, reliable emulation of native services over packet-switched networks.

    COMMENTS

    WORDPRESS: 0
    DISQUS: 0