• Home
  • QUESTIONS & ANSWERS
  • Others
  • What assumptions are made by the LPHU algorithm?

    * Question

    What assumptions are made by the LPHU algorithm?

    * Answer

    The LPHU (Likely Local Peak / Harmonic Unfolding) algorithm is typically used in signal processing for peak detection and harmonic analysis. Its operation relies on several underlying assumptions:

    1. Local Peak Existence:
    • The algorithm assumes that significant signal features appear as local peaks within the sampled data.
    • Noise or minor fluctuations are treated as non-relevant, and a threshold may be applied to distinguish true peaks.
      1. Harmonic Relationships:
    • Harmonics in the signal are assumed to be integer multiples of a fundamental frequency.
    • The algorithm uses this assumption to “unfold” overlapping harmonics and correctly identify their amplitudes and positions.
      1. Quasi-Stationarity of Signal:
    • The signal is assumed to be locally stationary over the analysis window, meaning its frequency content does not change drastically within the sampled segment.
    • This ensures reliable peak detection and harmonic mapping.
      1. Noise Characteristics:
    • Noise is assumed to be additive and relatively low compared to signal peaks, allowing the algorithm to distinguish true peaks from random fluctuations.
      1. Sampling Adequacy:
    • The data must be sampled at a rate high enough to capture relevant peaks without aliasing.
    • Undersampling may lead to missed peaks or misidentified harmonics.

    Summary:
    The LPHU algorithm operates under the assumptions that the signal contains distinguishable local peaks, harmonics follow integer multiples of a fundamental, and the signal is locally stationary with manageable noise. These assumptions allow it to effectively detect and unfold peaks for further spectral or feature analysis.