• Home
  • QUESTIONS & ANSWERS
  • Crystals and Oscillators
  • Why is quartz crystal resonator called quartz?

    * Question

    Why is quartz crystal resonator called quartz?

    * Answer

    A quartz crystal resonator is called quartz because it is made from quartz (silicon dioxide, SiO₂), a naturally occurring mineral known for its piezoelectric properties. The term “resonator” refers to its ability to oscillate or resonate at a specific frequency when an electrical voltage is applied.

    Here’s why quartz is used and why the name is associated with the resonator:

    1. Quartz as a Material
      Quartz is a crystalline form of silicon dioxide, found abundantly in nature. It has remarkable mechanical and electrical properties that make it suitable for resonators. One key feature of quartz is its piezoelectric effect, which means that it generates an electrical charge when subjected to mechanical stress and, conversely, changes shape when an electric field is applied.
    2. Piezoelectric Properties
      The piezoelectric properties of quartz allow it to convert electrical energy into mechanical vibrations and vice versa. When a voltage is applied across a quartz crystal, it deforms slightly, causing the crystal to vibrate at a specific frequency. This property is used in quartz crystal resonatorsto generate a stable frequency for timing applications, such as in watches, clocks, and oscillators.
    3. Stability and Precision
      Quartz is chosen for its high stabilityand precision in frequency control. Quartz crystals maintain their resonant frequency with minimal drift, making them ideal for applications where accurate and reliable timing is essential.

    Thus, the resonator is called “quartz” because the device is made from quartz crystals, which are the essential material enabling the precise and stable oscillations needed for its resonating function.