• Home
  • QUESTIONS & ANSWERS
  • Programmer, development system
  • What is the basic illumination process of an OLED display?

    * Question

    What is the basic illumination process of an OLED display?

    * Answer

    OLED (Organic Light-Emitting Diode) technology produces light through an electroluminescence process in organic semiconductor materials.
    When an electric current passes through the OLED layers, electrons and holes recombine to emit photons—creating visible light directly without the need for a backlight.

    1. Structure Overview

    An OLED device typically consists of multiple thin organic layers sandwiched between two electrodes:

    • Anode (positive electrode)
    • Cathode (negative electrode)
      Between them are functional layers:
    • Hole Injection Layer (HIL)
    • Hole Transport Layer (HTL)
    • Emissive Layer (EML)
    • Electron Transport Layer (ETL)

    Each layer performs a specific role in charge injection, transport, and recombination.

    2. Illumination Process

    The illumination of an OLED can be summarized in four main steps:

    1. Charge Injection:
      When voltage is applied, the anode injects holes(positive charge carriers) into the HTL, while the cathode injects electrons into the ETL.
    2. Charge Transport:
      These charges move toward the emissive layer under the influence of the electric field.
    3. Recombination and Exciton Formation:
      At the interface of the HTL and ETL—within the emissive layer—electrons and holes recombine to form excitons, which are excited energy states of the organic molecules.
    4. Light Emission:
      When these excitons relax to their ground state, they release energy as visible photons.
      The emitted light passes through the transparent anode (often made of indium tin oxide, ITO) and the substrate to produce visible illumination.

    3. Color Generation

    The emission color depends on the organic material used in the emissive layer.
    Different organic compounds emit red, green, or blue light, and by combining them, full-color OLED displays can be achieved.
    Advanced designs, such as white OLEDs (WOLEDs) with color filters or stacked RGB structures, enhance color accuracy and brightness.

    4. Efficiency and Performance

    Since each pixel emits its own light, OLED displays feature:

    • High contrast ratio(true blacks)
    • Wide viewing angles
    • Fast response time
    • Lower power consumptionfor dark images

    However, challenges remain in lifetime and burn-in effects, especially for blue-emitting materials.

    Summary Insight

    The illumination of an OLED is driven by electrical excitation and radiative recombination within organic thin films.
    This self-emissive mechanism eliminates the need for a backlight—making OLEDs thinner, more efficient, and visually superior compared to traditional LCDs.
    The same fundamental principle supports innovations such as flexible, transparent, and micro-OLED displays, widely used in modern consumer and industrial electronics.

    COMMENTS

    WORDPRESS: 0
    DISQUS: 0