• Home
  • Q&A
  • Inductors, Coils, Chokes
  • What is magnetic permeability?

    * Question

    What is magnetic permeability?

    * Answer

    Magnetic permeability is a fundamental physical property that describes how easily a material can become magnetized or how well it can support the formation of a magnetic field within itself.

    1. Definition

    Magnetic permeability, denoted by the symbol μ, is defined as the ratio of the magnetic flux density (B) to the magnetic field strength (H):

    B=μH

    Where:

    B is the magnetic flux density (in teslas, T)

    H is the magnetic field strength (in amperes per meter, A/m)

    μ is the permeability of the material (in henries per meter, H/m)

    2. Types of Permeability

    Absolute Permeability (μ): The total permeability of a material, including the effect of vacuum.

    Vacuum Permeability (μ₀): Also called the permeability of free space, a physical constant:

    μ0=4π×10−7 H/m

    Relative Permeability (μᵣ): The ratio of a material’s permeability to that of free space:

    μr=μ/μ0

    3. Material Classification Based on Permeability

    Material Type

    Relative Permeability (μᵣ)

    Characteristics

    Diamagnetic

    Slightly less than 1

    Weakly repelled by magnetic fields

    Paramagnetic

    Slightly more than 1

    Weakly attracted by magnetic fields

    Ferromagnetic

    Much greater than 1 (up to 10⁵ or more)

    Strongly attracted and can retain magnetization

    4. Applications

    Transformers and Inductors: High-permeability materials enhance magnetic coupling and inductance.

    Magnetic Shielding: Materials like mu-metal with high μ are used to block or redirect magnetic fields.

    Electric Motors and Generators: Cores are made from ferromagnetic materials to improve magnetic efficiency.

    Sensors and Magnetic Circuits: Precise control of field response depends on the permeability of the medium.

    5. Important Considerations

    Nonlinearity: In ferromagnetic materials, permeability is not constant and changes with field strength.

    Temperature Dependence: Permeability can change with temperature, especially near a material’s Curie point.

    Frequency Effects: At high frequencies, effective permeability may decrease due to eddy currents and skin effect.

    Summary:
    Magnetic permeability determines how well a material can carry magnetic lines of force. It is essential in designing and analyzing electromagnetic devices such as inductors, transformers, motors, and magnetic shielding systems.