• Home
  • QUESTIONS & ANSWERS
  • Others
  • What are the characteristics and principles of photoconductive relays?

    * Question

    What are the characteristics and principles of photoconductive relays?

    * Answer

    Photoconductive relays, also known as photoMOS relays or solid-state relays (SSRs), are electronic switching devices that operate based on the photoconductive effect. They use light—usually from an LED—to activate a photoconductive element, such as a photodiode array or a phototransistor, to switch electrical signals without mechanical movement.

    Principle of Operation

    At the heart of a photoconductive relay is the opto-isolation mechanism:

    Input Signal Activation:

    A low-voltage control signal energizes an internal LED.

    The LED emits infrared light proportional to the input current.

    Photo Response:

    The light activates a photodiode array or phototransistor on the output side.

    This change triggers a MOSFET array or similar semiconductor switch to conduct.

    Load Switching:

    The conducting MOSFETs form a closed path for the external circuit, effectively turning the switch “ON.”

    When the input signal is removed, the LED turns off, the photodetector stops conducting, and the switch opens.

    This enables electrical isolation between the control (input) and load (output) circuits.

    Key Characteristics

    1. No Mechanical Contacts

    Silent operation.

    No wear and tear, resulting in long operational life.

    2. Fast Switching Speed

    Typically in the microsecond to millisecond range.

    Ideal for applications requiring precise timing.

    3. Electrical Isolation

    Galvanic isolation between control and load sides (usually >1500V).

    Enhances safety and minimizes electrical noise interference.

    4. Compact Size

    Smaller footprint than mechanical relays.

    Suitable for miniaturized circuit boards and dense assemblies.

    5. Low Power Consumption

    Requires minimal input current to activate (often <5 mA).

    Excellent for battery-powered or energy-sensitive applications.

    6. AC and DC Switching

    Depending on the internal design, some photoMOS relays can handle both AC and DC loads.

    Dual-MOSFET designs allow bidirectional current flow.

    Applications

    Test and measurement equipment

    Medical devices

    Telecommunication systems

    Industrial automation

    Signal routing in multiplexers

    Security and surveillance systems