The Industrial Internet of Things (IIoT) has become a transformative force in the industrial sector, bringing unprecedented connectivity and intelligence to machinery and processes. At the heart of IIoT applications lie critical components like limit switches.
And, with the D4N-2B2H Limit Switch emerging as a key player in enhancing operational efficiency and reliability.
D4N-2B2H Limit Switch Overview
The D4N-2B2H Limit Switch represents a pinnacle of engineering prowess, specifically tailored to meet the demanding requirements of industrial applications. Let’s examine its design, specifications, and features that make it a cornerstone in industrial automation.
Design and Construction
The D4N-2B2H Limit Switch boasts a meticulously crafted design that combines durability with precision. Its robust construction ensures resilience in harsh industrial environments.
The switch’s housing is engineered to withstand mechanical stress, vibrations, and temperature variations, making it a stalwart component in machinery where reliability is paramount. The attention to detail in the design reflects a commitment to longevity and consistent performance.
Key Features
Current Rating and Voltage Specifications: The D4N-2B2H exhibits a remarkable current rating of 3A for AC and 270mA for DC, attesting to its capacity to handle a diverse range of electrical loads. With voltage ratings of 240V (AC) and 250V (DC), the switch is not only versatile but also adaptable to a variety of industrial power systems.
Actuator Type: The switch’s side rotary, adjustable roller actuator type provides a dynamic range of motion, allowing for precise control and positioning. This adaptability makes the D4N-2B2H suitable for applications where nuanced adjustments are critical.
Mounting Excellence: Designed for chassis mounting, the D4N-2B2H ensures a secure and stable installation. This mounting type enhances the switch’s reliability in fixed industrial setups, contributing to its role as a dependable control element.
Termination Style: Featuring a screw terminal termination style, the switch facilitates easy and efficient installation. This user-friendly design ensures that integration into existing industrial systems is both straightforward and secure.
Ingress Protection: The D4N-2B2H boasts an impressive IP67 rating, signifying its resistance to dust and water. This ingress protection ensures the switch’s continued functionality in environments where exposure to particles and moisture is a constant challenge.
Specialized Features: The inclusion of a metal lever and rubber roller adds a layer of versatility to the D4N-2B2H. The metal lever contributes to the switch’s overall robustness, while the rubber roller enhances its adaptability to different surfaces and materials.
Performance Characteristics
Reliability: The D4N-2B2H is engineered for reliability, exhibiting consistent performance even in demanding operational conditions. Its robust design and materials contribute to a long operational life, reducing the need for frequent replacements and maintenance.
Durability: With an operating force of 459gf and a release force of 41gf, the switch strikes a balance between responsiveness and durability. This durability is a testament to its ability to withstand mechanical stress, providing a dependable solution for continuous operation in industrial settings.
Environmental Considerations:
The D4N-2B2H’s design takes into account the diverse environmental challenges found in industrial settings. From temperature variations to exposure to contaminants, the switch’s construction ensures optimal performance, contributing to its longevity and operational stability.
Integration with IIoT
The seamless integration of the D4N-2B2H Limit Switch with Industrial Internet of Things (IIoT) ecosystems is pivotal for harnessing the full potential of modern industrial automation. This section delves deeper into the various facets of how the D4N-2B2H contributes to and enhances the connectivity and intelligence of IIoT applications.
Communication Protocols
The D4N-2B2H Limit Switch is designed to effortlessly interface with prevalent IIoT communication protocols, ensuring compatibility and interoperability within diverse industrial environments. Its adeptness with standards such as MQTT (Message Queuing Telemetry Transport) and CoAP (Constrained Application Protocol) facilitates seamless communication with other IIoT devices and platforms.
Wireless Connectivity Options
Facilitating a wire-free connectivity paradigm, the D4N-2B2H integrates advanced wireless technologies, including Wi-Fi and Bluetooth. This wireless capability not only simplifies installation and configuration but also allows for greater flexibility in the placement of the switch within industrial setups. The elimination of physical wiring constraints enhances the adaptability of the switch to dynamic and evolving industrial landscapes.
Data Transmission and Reception
The real-time data streaming capabilities of the D4N-2B2H are pivotal in providing instantaneous feedback and insights. Whether it’s monitoring equipment status or tracking operational parameters, the switch ensures that critical data is transmitted promptly. Moreover, the switch’s low-latency characteristics guarantee that the information reaches the IIoT platform swiftly, enabling timely decision-making and response.
Cybersecurity Measures
As IIoT environments become increasingly interconnected, ensuring the security of data transmissions is paramount. The D4N-2B2H addresses this concern by incorporating robust encryption mechanisms and advanced authentication protocols. These security measures not only safeguard sensitive data but also mitigate the risks associated with unauthorized access and cyber threats, ensuring the integrity of IIoT operations.
Edge Computing Capabilities
In addition to its role as a data transmitter, the D4N-2B2H Limit Switch can contribute to edge computing within IIoT architectures. By processing data at the edge of the network, closer to the source of generation, the switch minimizes latency and bandwidth usage. This distributed computing approach enhances the efficiency of IIoT systems, particularly in scenarios where real-time analysis and decision-making are critical.
Remote Monitoring and Control
The integration of the D4N-2B2H with IIoT facilitates remote monitoring and control capabilities. Through cloud-based platforms, operators can access real-time data, receive alerts, and even remotely control equipment based on the inputs provided by the limit switch. This feature proves invaluable in scenarios where immediate responses to changing conditions are essential for maintaining operational efficiency and safety.
All in all, the D4N-2B2H Limit Switch’s integration with IIoT is multifaceted, encompassing communication protocols, wireless connectivity, real-time data transmission, cybersecurity, edge computing, and remote monitoring. This holistic approach positions the switch as a cornerstone in the evolution of smart and connected industrial systems.
The D4N-2B2H Limit Switch stands as a cornerstone in the evolution of IIoT. Its durability, versatility, and seamless integration capabilities make it an indispensable component in industrial settings, driving efficiency, safety, and innovation in the Fourth Industrial Revolution.
WIN SOURCE plays a pivotal role in the accessibility and distribution of cutting-edge industrial components, such as the D4N-2B2H Limit Switch. As an essential element in the evolution of the Industrial Internet of Things (IIoT), the D4N-2B2H Limit Switch, available through WIN SOURCE, stands out for its remarkable durability, versatility, and seamless integration capabilities.
© 2025 Win Source Electronics. All rights reserved. This content is protected by copyright and may not be reproduced, distributed, transmitted, cached or otherwise used, except with the prior written permission of Win Source Electronics.

COMMENTS