In today’s world, where technology is an integral part of our lives, batteries play a crucial role in keeping our devices functional and portable.
One such battery type that has gained prominence is the CR1632 battery. In this article, our components experts here at WIN-SOURCE will delve into the world of CR1632 batteries, exploring their features, applications, advantages, and how they compare to other battery options.
First, let’s get the mini takeaway before we head into more details.
CR1632 batteries are compact lithium coin cell batteries measuring 16mm in diameter and 3.2mm in height. They offer stable voltage, long shelf life, and a low self-discharge rate, making them suitable for various applications like watches, remote controls, wearables, and medical devices.
So with the short answer in place let’s find out more about these power-packed cells.
Table of Contents
ToggleWhat are CR1632 Batteries?
CR1632 batteries are lithium coin cell batteries that belong to the CR series.
They derive their name from their dimensions: 16mm in diameter and 3.2mm in height.
These compact dimensions make them ideal for small devices and applications where space is limited.
The best CR1632 batteries are known for their high energy density, which allows them to provide a reliable and long-lasting power source.
“They derive their name from their dimensions: 16mm in diameter and 3.2mm in height.”
Features and Specifications
1. Voltage and Capacity
CR1632 batteries typically operate at a nominal voltage of 3V.
This voltage remains stable throughout most of its lifespan, ensuring consistent performance in devices.
Despite their compact size, CR1632 batteries boast a respectable capacity that allows them to power devices for extended periods.
2. Chemistry
These batteries utilize a lithium manganese dioxide (Li-MnO2) chemistry, which offers a good balance between energy density, shelf life, and safety.
The chemistry ensures a gradual discharge curve, meaning the voltage remains relatively constant until the battery is nearly depleted.
3. Self-Discharge Rate
CR1632 batteries have a low self-discharge rate, which is the rate at which a battery loses its charge when not in use.
This characteristic makes them well-suited for devices that may be used infrequently, such as remote controls, watches, and calculators.
4. Temperature Tolerance
Lithium coin cell batteries, including CR1632, exhibit good temperature tolerance.
They can operate efficiently in a wide range of temperatures, making them suitable for both indoor and outdoor applications.
So what can you use these compact high-powered cells for?
Read on to discover more.
Uses of CR1632 Batteries
CR1632 batteries find application in a diverse range of devices due to their compact size and reliable power delivery. Some common applications include:
1. Watches and Clocks
CR1632 batteries are commonly used to power wristwatches, wall clocks, and other timekeeping devices. Their stable voltage and long shelf life ensure accurate timekeeping over an extended period.
2. Remote Controls
TV remotes, garage door openers, and other remote-controlled devices benefit from CR1632 batteries. The low self-discharge rate means the battery will be ready for use even after long periods of inactivity.
3. Fitness Trackers and Wearables
As wearables gain popularity, CR1632 batteries play a crucial role in powering devices like fitness trackers, heart rate monitors, and smart jewelry.
Their small size makes them ideal for such compact devices.
4. Medical Devices
CR1632 batteries are also used in various medical devices, such as glucose meters, thermometers, and hearing aids.
Stable voltage output is essential for accurate readings and consistent performance.
If you are procuring power for the medical, aerospace or automation industries, contact our expert team members for a quote.
5. Calculators and Electronics
Small electronics like calculators, key fobs, and digital thermometers often rely on CR1632 batteries.
Their compact dimensions make them a suitable choice for devices where space is limited.
Advantages of CR1632 Batteries
So what are the advantages of these mini cells and what are the benefits of using them?
● 1. Size and Form Factor: The compact size and form factor of CR1632 batteries make them versatile for a wide range of devices, from the smallest electronics to wearable gadgets.
● 2. Long Shelf Life: CR1632 batteries have an impressive shelf life, often retaining their charge for several years. This makes them a reliable choice for devices that may not be used frequently.
● 3. Consistent Performance: The stable voltage output of CR1632 batteries ensures consistent performance throughout their lifespan. This is particularly important for devices that require accurate and steady power delivery.
● 4. Temperature Stability: CR1632 batteries are designed to function well across various temperature ranges, making them suitable for both indoor and outdoor applications.
● 5. Low Self-Discharge: Their low self-discharge rate contributes to a longer overall lifespan, making CR1632 batteries an economical choice for devices that aren’t used daily.
So are there any batteries similar to a CR1632 battery? Let’s take a look at two of their nearest rivals and how they compare with the
CR1616 Battery
Due to its larger size, the CR1632 battery generally offers a higher capacity, making it well-suited for devices that demand more energy.
On the other hand, the best CR1616 batteries are better suited for low-power devices or those that don’t require sustained high energy output.
Both batteries find applications in devices such as remote controls and small electronics.
However, the CR1632 battery’s larger capacity makes it more versatile for devices like fitness trackers and medical instruments that require more power over an extended period as we discovered above.
CR2032 batteries
The most apparent difference between CR1632 and CR2032 batteries is their diameter.
CR2032 batteries are larger in diameter than CR1632 batteries.
However, they share the same height. This difference in size directly affects their capacity and the devices they can power.
Both CR1632 and the best CR2032 batteries have overlapping applications, including watches, fitness trackers, remote controls, wearables, and medical devices.
CR2032 batteries, with their higher capacity, could be better suited for powering electronic toys and devices with higher energy demands.
Where can I buy the best CR1632 Batteries?
As we’ve discovered these powerhouses, packed into a compact form, become your go-to solution for a diverse array of devices.
With a petite frame, extended shelf life, rock-steady voltage delivery, and the ability to brave extreme temperatures, CR1632 batteries become the life force of watches, remote controls, wearables, medical marvels, and pint-sized electronics.
To embark on this electrifying journey, look no further than WIN SOURCE – your trusted partner for all things batteries.
Our power solutions ignite performance and reliability, propelling your devices into an unparalleled realm of efficiency. So check out our store today. With WIN SOURCE, the power to fuel your world is just a click away.

COMMENTS