Relays play a pivotal role in diverse industries, serving as indispensable components in applications ranging from telecommunications to industrial automation. They help control a circuit by an independent low-power signal or where several circuits must be controlled by one signal. Amidst the various relay types, one noteworthy variant is the latching relay, renowned for its unique advantages.
Contrary to other relays, latching or stay relays can maintain their state even when the power is removed. This distinctive feature makes them highly sought after in scenarios where energy efficiency, long-term stability, and precise control are paramount.
Let’s explore latching relays’ mechanisms, applications, and benefits for a wide range of industries.
What is a Latching Relay?
A stay or latching relay is a type of relay that can stay in a particular switched state without continuous power. It uses a magnetic mechanism to latch and unlatch, holding its position until triggered to change. They efficiently control a substantial current using a smaller one, and their coil consumes power solely during ON state, making it energy-efficient.
Types of Latching Relays
Here are some common types of latching relays:
Mechanical Latching Relay
This type of relay employs a mechanical mechanism to maintain its switched state without continuous power. It uses physical means to latch and unlatch, providing stability without electrical power.
Magnetic Latching Relay
Magnetic latching relays utilize magnetic fields to control the latching and unlatching process. They rely on the magnetic force to keep the relay in a specific state, minimizing energy consumption.
Electronic Latching Relay
Electronic relays leverage electronic circuits to control the switching mechanism. They often incorporate semiconductor devices to achieve latching and unlatching, providing precise control over the relay’s state.
Single Coil Latching Relay
Single-coil relays use a single coil to control both the latching and unlatching actions. By reversing the coil’s polarity, these relays can toggle between states without requiring a separate coil for each function.
How Does A Latching Relay Work?
Let’s look at the components and working of a latching or stay relay:
An electric current goes through the coil of the latching relay’s electromagnet.
This electric current produces a magnetic field around the coil.
The magnetic field either opens or closes the switch, determined by the coil’s orientation.
Even after power is disconnected from the coil, the internal mechanism of the latching relay maintains the switch in its current position – open or closed.
Latching Vs. Non-Latching Relay
Here’s a comparison between Latching and Non-Latching relays:
Definition
Latching Relay: Utilizes a latching mechanism to maintain a set or reset state without continuous power.
Non-Latching Relay: The non-latching relay, typically a standard mechanical relay, requires a continuous current in its winding to sustain its contact position.
Energy Efficiency
Latching Relay: More energy-efficient; consumes power only during state transitions.
Non-Latching Relay: This may be less energy-efficient as it requires continuous power for state maintenance.
Noise
Latching Relay: Generally quieter due to the absence of constant coil energization.
Non-Latching Relay: This may produce a constant humming noise when continuously energizing the coil.
Best Relay Options You Can Go For!
Here are some of the best relay options you can try for various applications:
70M-IDC5G
The 907784-70M-IDC5G is an AC/DC input relay meticulously crafted for I/O relay modules within the esteemed 70 series. Its 5VDC voltage output and 10mA current output operate within an input voltage range of 35 to 60VAC/DC, with a minimal current input of 6mA. The 907784-70M-IDC5G ensures swift and precise operation with a commendable turn-on and turn-off time of 10ms, making it a reliable choice for applications demanding efficiency.
G7SA-2A2B-DC24
The Omron 872564-G7SA-2A2B-DC24 is a safety relay belonging to the G7SA series, engineered for robust performance and reliability. This safety relay boasts a 4PST-2NO/2NC contact form, providing versatile switching options for diverse applications. With a coil voltage of 24VDC and a coil resistance of 1.6 kOhms, it combines efficient operation with precise control.
Applications of Latching or Stay Relays
Latching relays are very popular, and their market size is expected to hit USD 14.7 billion by 2030. Here are a few very important applications of latching relays:
HVAC, Refrigeration, and Anti-Condensation Systems: Latching relays play a crucial role in HVAC systems, refrigeration units, and anti-condensation systems, ensuring effective temperature control and energy efficiency.
Power Supplies: In power supplies, latching relays efficiently manage the current flow, providing a stable and energy-conscious solution for various electronic devices.
Industrial Counting and Sorting Systems: Latching relays have applications in industrial counting and sorting systems, contributing to precise and reliable control in manufacturing processes.
Commercial Coffee Machines and Food Preparation Equipment: Latching relays find a place in commercial coffee machines and other automated food preparationequipment, supporting precise control and reliable performance in these applications.
Benefits of Latching or Stay Relays
Let’s look at the many benefits of a latching or stay relay:
Pulse Excitation and Coil Options
Latching relays operate with pulse excitation, meaning they only require a short electrical pulse to change states. Additionally, they offer flexibility with the option to work with either a single or double coil, providing adaptability in various circuit designs.
Compact Size and PCB Installation
Latching relays are characterized by their small size, making them ideal for limited space applications. Their compact design allows easy integration onto Printed Circuit Boards (PCBs), enabling efficient use of available space and facilitating streamlined electronic designs.
Low Power Consumption and High Load Capacity
One of the key benefits of latching relays is their low power consumption. They consume power only during state changes, contributing to energy efficiency. However, despite their energy-conscious operation, latching or stay relays exhibit a robust load capacity, making them suitable for handling significant electrical loads.
Latching relays can easily stay in one state without a continuous power supply. They are advantageous in scenarios or applications where efficiency and precise control are necessary. Some common examples include food preparation equipment, power supplies, and more. However, finding a high-quality latching or stay relay isn’t an easy task. If you are facing obstacles while trying to search for the best relay suppliers, contact WIN SOURCE.
We have a network of manufacturers who offer authentic and durable relays. We will help you connect with them and grab the needed electronics while assisting in matters like delivery and pricing. Get in touch with us now and take the efficiency of your machinery to the next level!
© 2024 Win Source Electronics. All rights reserved. This content is protected by copyright and may not be reproduced, distributed, transmitted, cached or otherwise used, except with the prior written permission of Win Source Electronics.

COMMENTS