1 … 292 293 294 295 296 … 374 2940 / 3740 POSTS

What are the advantages of a contactless IC card (electronic tag) compared to a contact IC card?

* Question What are the advantages of a contactless IC card (electronic tag) compared to a contact IC card? * Answer (1) High reliability: i [...]

What are the methods of current transformer ratio test?

* Question What are the methods of current transformer ratio test? * Answer The current transformer is a special transformer specially used [...]

What are the two major categories of memory?

* Question What are the two major categories of memory? * Answer From the perspective of the access function of the memory, the memory has t [...]

What is the way the crystal oscillator of the LPC2000 series ARM generates a clock?

* Question What is the way the crystal oscillator of the LPC2000 series ARM generates a clock? * Answer LPC2000 series ARM crystal oscillato [...]

What are the MC9S12XE series microcontroller features?

* Question What are the MC9S12XE series microcontroller features? * Answer (1) XGATE coprocessor, which can virtualize external devices and [...]

What is the external photoelectric effect?

* Question What is the external photoelectric effect? * Answer Under the action of light, the electrons in the object escape from the surfac [...]

What are the two general corrosion methods that can be used for MEMS geometry?

* Question What are the two general corrosion methods that can be used for MEMS geometry? * Answer There are generally two methods of etchin [...]

What is the open circuit detection method?

* Question What is the open circuit detection method? * Answer 1 Turn off the ignition switch, remove the wiring connector of the vane air f [...]

What are the advantages of a network power controller?

* Question What are the advantages of a network power controller? * Answer 1 More management rights are allocated to users, which fundamenta [...]

What is a pulse modulation measurement circuit?

* Question What is a pulse modulation measurement circuit? * Answer A circuit that measures the amount of pulse output in a measurement circ [...]
1 … 292 293 294 295 296 … 374 2940 / 3740 POSTS