1 … 291 292 293 294 295 … 374 2930 / 3740 POSTS

Knowledge about thermistors

* Question Knowledge about thermistors * Answer The physical characteristics of the thermistor are represented by the following parameters: [...]

Can the resistance of a capacitor or battery be determined using any of several methods?

* Question Can the resistance of a capacitor or battery be determined using any of several methods? * Answer 1) 侬 drop at the beginning of c [...]

What are the components of the sensor?

* Question What are the components of the sensor? * Answer Sensitive component, conversion component and basic conversion circuit are compos [...]

What are the main parameters of the inductor?

* Question What are the main parameters of the inductor? * Answer (1) Inductance 1 Definition of inductance: Inductance is a physical quanti [...]

What is the magnetoresistance effect?

* Question What is the magnetoresistance effect? * Answer The internal resistance of the Hall element increases as the absolute value of the [...]

What are the methods and reasons for solving the “cross effect” in the organic electroluminescence dynamic driving method?

* Question What are the methods and reasons for solving the "cross effect" in the organic electroluminescence dynamic driving method? * Answer [...]

What are the classifications of labels by energy source classification?

* Question What are the classifications of labels by energy source classification? * Answer 1 Active tag active tags are also known as activ [...]

In infrared technology, which four areas are generally divided into infrared radiation?

* Question In infrared technology, which four areas are generally divided into infrared radiation? * Answer In infrared technology, infrared [...]

What are the main features of the latest secondary side synchronous rectification control IC – NCP4303?

* Question What are the main features of the latest secondary side synchronous rectification control IC - NCP4303? * Answer (1) Realize sync [...]

What are the two meanings of the antenna port output power?

* Question What are the two meanings of the antenna port output power? * Answer The output power of the antenna port may have two meanings: [...]
1 … 291 292 293 294 295 … 374 2930 / 3740 POSTS