1 … 300 301 302 303 304 … 374 3020 / 3738 POSTS

What is the test principle of COS?

* Question What is the test principle of COS? * Answer (1) The test requirements are detailed and comprehensive, and all functions of the ca [...]

What is the role of the source module?

* Question What is the role of the source module? * Answer The purpose of the source module is to provide a local oscillator (Local Oscillat [...]

What is the procedure for sending an address?

* Question What is the procedure for sending an address? * Answer Set TXWAKE = 1 and write the appropriate address value to the Transmit Dat [...]

What are the environmental factors affecting the sensor?

* Question What are the environmental factors affecting the sensor? * Answer The influence of environmental factors on the sensor is in addi [...]

What is the difference between a normal power inductor and a high current inductor?

* Question What is the difference between a normal power inductor and a high current inductor? * Answer The difference between ordinary powe [...]

What are the basic components of an FPGA?

* Question What are the basic components of an FPGA? * Answer (1) Configurable Logic Blocks (CLB). (2) Programmable input/output modules (I [...]

What are the development tools for supporting 2802x-based applications?

* Question What are the development tools for supporting 2802x-based applications? * Answer ● CodeComposerStudi0 integrated development enviro [...]

What types of embedded processors can be divided into?

* Question What types of embedded processors can be divided into? * Answer According to the current situation, embedded processors can be di [...]

What is the impact of the feedback on the amplifier?

* Question What is the impact of the feedback on the amplifier? * Answer Related to the way the feedback is added: 1. Current series negati [...]

What are the layers of OLEDoS?

* Question What are the layers of OLEDoS? The structure of the OLEDoS: First, a high work function metal is deposited on the monocrystalline silic [...]
1 … 300 301 302 303 304 … 374 3020 / 3738 POSTS