1 … 303 304 305 306 307 … 374 3050 / 3738 POSTS

Briefly describe the MSDMA features?

* Question Briefly describe the MSDMA features? * Answer MSDMA supports storage data scaling, in particular two different image data for Pic [...]

What functions does the reader have?

* Question What functions does the reader have? * Answer Provide energy to the tag, realize communication with the electronic tag, realize c [...]

What characteristics should medical sensors have?

* Question What characteristics should medical sensors have? * Answer Medical sensors should have the following characteristics: (1) High e [...]

What are the problems with DLC films?

* Question What are the problems with DLC films? * Answer (1) The film and the base bond strength are poor. (2) The thickness of the diamon [...]

What is SPC3 memory allocation?

* Question What is SPC3 memory allocation? * Answer The internal latch/register is located in the first 22 bytes and can be read or written [...]

In the design, if you need to adjust the brightness of the LED, how can you achieve LED brightness adjustment?

* Question In the design, if you need to adjust the brightness of the LED, how can you achieve LED brightness adjustment? * Answer (1) Analo [...]

What kinds of currents can be divided according to their size and direction?

* Question What kinds of currents can be divided according to their size and direction? * Answer (1) A current whose direction does not chan [...]

What are the main characteristic parameters of the CCD device?

* Question What are the main characteristic parameters of the CCD device? * Answer The main characteristic parameters of CCD devices include [...]
IRF520NPBF Power MOSFET

IRF520NPBF Power MOSFET

The electronics revolution started in the true sense with the invention of the transistor. Further advancements in the transistor technolo [...]

Why does the piezoelectric component application have to accompany the diode?

* Question Why does the piezoelectric component application have to accompany the diode? * Answer Piezoelectric elements have piezoelectric [...]
1 … 303 304 305 306 307 … 374 3050 / 3738 POSTS