1 … 348 349 350 351 352 … 374 3500 / 3738 POSTS

What is a mixer?

* Question What is a mixer? * Answer Mixing is a frequency conversion process that transforms the carrier frequency in the modulated wave to [...]

What are the characteristics of random access memory?

* Question What are the characteristics of random access memory? * Answer The random access memory can read or write information at any time [...]

What is the physical basis of the photoelectric sensor?

* Question What is the physical basis of the photoelectric sensor? * Answer The physical basis of photoelectric sensors is the photoelectric [...]

What are the differences between FPGA and ASIC?

* Question What are the differences between FPGA and ASIC? * Answer See page 7 Table 1.3 [...]

What are the aspects of embedded Flash programming?

* Question What are the aspects of embedded Flash programming? * Answer (1) Programmer Programming It is the most primitive method of progra [...]

What are the new and enhanced features of the Cyclone II device family?

* Question What are the new and enhanced features of the Cyclone II device family? * Answer Large capacity: Cyclone II devices range in capa [...]

What is the difference between an inductor and a transformer?

* Question What is the difference between an inductor and a transformer? * Answer The difference between the inductor and the transformer Th [...]

What are the functions of the 485BD?

* Question What are the functions of the 485BD? * Answer (1) Data transfer without protocol. (2) Data transfer of a proprietary protocol.Da [...]

What are the instructions for using the transformer parameters?

* Question What are the instructions for using the transformer parameters? * Answer (1) When replacing the transformer, it is necessary to r [...]

What are the three methods used for the spatial address of the 8051 program memory?

* Question What are the three methods used for the spatial address of the 8051 program memory? * Answer The first method: use the on-chip RO [...]
1 … 348 349 350 351 352 … 374 3500 / 3738 POSTS