1 … 355 356 357 358 359 … 374 3570 / 3738 POSTS

What is the protection scheme for the charging circuit of portable devices?

* Question What is the protection scheme for the charging circuit of portable devices? * Answer (1) Overvoltage phenomenon. In order to ensu [...]

What are the characteristics of the ARM1176JZF-S processor?

* Question What are the characteristics of the ARM1176JZF-S processor? * Answer Ultra-high-speed advanced microprocessor bus architecture (A [...]

The working principle and use of the fuse

* Question The working principle and use of the fuse * Answer The fuse is the simplest and most effective protection device, mainly used for [...]

What are the characteristics of the AT command set?

* Question What are the characteristics of the AT command set? * Answer The features are simple, efficient, uniform command format, and easy [...]

What is an AC motor?

* Question What is an AC motor? * Answer A power source that converts electrical energy into mechanical energy.Like a DC motor, an AC motor [...]

What features are integrated in the ISL8601?

* Question What features are integrated in the ISL8601? * Answer The ISL8601 also integrates a MOSFET driver circuit with built-in overcurre [...]

What are the characteristics of the three-axis accelerometer?

* Question What are the characteristics of the three-axis accelerometer? * Answer The three-axis accelerometer has the characteristics of lo [...]

What is the role of the inverter?

* Question What is the role of the inverter? * Answer The frequency converter is a device that converts a commercial frequency power supply [...]

Which events can also clear the flag of the CPU interrupt flag register?

* Question Which events can also clear the flag of the CPU interrupt flag register? * Answer CPU acknowledgement interrupt; 28x device reset [...]

What are the main processes for making electronic labels?

* Question What are the main processes for making electronic labels? * Answer 1.Chip manufacturing 2.Electronic label semi-finished product [...]
1 … 355 356 357 358 359 … 374 3570 / 3738 POSTS