1 … 357 358 359 360 361 … 374 3590 / 3738 POSTS

What function blocks are each macro unit made up of?

* Question What function blocks are each macro unit made up of? * Answer Each macrocell consists of three functional blocks: a logic array, [...]
NRF52832-QAA-R SoC Device

NRF52832-QAA-R SoC Device

In the past few decades electronics technology has witnessed a number of revolutionary advancements. The growth and advancement in the are [...]

What are the characteristics of Altera’s MAX II?

* Question What are the characteristics of Altera's MAX II? * Answer 1.Low power consumption 2.Low cost architecture 3.High performance [...]

What are the two methods of oscillating frequency versus noise reduction?

* Question What are the two methods of oscillating frequency versus noise reduction? * Answer 1 with a lower frequency, so easy to filter; [...]

What are the characteristics of photodiodes?

* Question What are the characteristics of photodiodes? * Answer (1) Spectral characteristics (2) Lighting characteristics [...]

Which conditions should UCC28950 meet first before starting?

* Question Which conditions should UCC28950 meet first before starting? * Answer (1) The VDD voltage must exceed the UVL0 threshold (7.3V). [...]

What is the difference between an inductor and a magnetic bead?

* Question What is the difference between an inductor and a magnetic bead? * Answer Inductors and magnetic beads are two different concepts. [...]

What constitutes the ignition control circuit?

* Question What constitutes the ignition control circuit? * Answer (1) Crankshaft speed sensor (2) Ignition control circuit analysis (3) [...]

How does the interrupt control register change?

* Question How does the interrupt control register change? * Answer The interrupt control register must be changed at a location where the i [...]

How to create more value for the vast majority of end users in non-portable and battery-powered applications?

* Question How to create more value for the vast majority of end users in non-portable and battery-powered applications? * Answer By reducin [...]
1 … 357 358 359 360 361 … 374 3590 / 3738 POSTS