![]() Figure 1 AD8675ARMZ-REEL device package |
![]() Figure 2 AD8675ARMZ-REEL schematic symbol
|
What is AD8675ARMZ-REEL?
The AD8675ARMZ-REEL is a precision operational amplifier. The AD8675ARMZ-REEL has ultralow offset and low offset voltage drift. It also has low voltage noise combined with very low input bias currents over the full operating temperature range. The AD8675ARMZ-REEL is specified for the extended industrial temperature range (−40°C to +125°C).
Pin Configuration
Table 1 PIN Configuration
| PIN NO. | LABLE | DESCRIPTION |
| 1 | NULL | Offset null pin used to eliminate the offset voltage and balance the input voltages. |
| 2 | -IN | Inverting signal input |
| 3 | +IN | Noninverting signal input |
| 4 | V- | Negative supply voltage |
| 5 | NC | No Connect, should be left floating |
| 6 | OUT | Amplified signal output |
| 7 | V+ | Positive supply voltage |
| 8 | NULL | Offset null pin used to eliminate the offset voltage and balance the input voltages. |
Features
- Very low voltage noise (2.8 nV/√Hz)
- Very low offset voltage
- Very high gain of 120 dB
- Rail-to-rail output swing
- Low input bias current
- ±5 V to ±18 V operation
- Wide bandwidth of 10 MHz
Applications
- Medical instrumentation
- Strain gage amplifiers
- Audio
- Laser diode control loops
- Precision instrumentation
ALTERNATIVES FOR AD8675ARMZ-REEL
| Supply Voltage: 10V ~ 36V, ±5V ~ 18V | |||
| Product | Slew Rate(V/µs) | Input Bias Current | Input Offset Voltage(µV) |
| AD8675ARMZ-REEL | 2.5 | 2nA | 10 |
| ADA4001-2ARZ-R7 | 25 | 20pA | 500 |
| AD8676ARMZ-REEL | 2.5 | 2nA | 100 |
| AD8676BRMZ-REEL | 2.5 | 2nA | 60 |
| PGA281AIPWR | 1 | 300pA | 5 |
WHERE TO USE AD8675ARMZ-REEL?
AD8675ARMZ-REEL is an op-amp which can be used as an operational amplifier (In linear region) or as a switch (In non-linear region). AD8675ARMZ-REEL as an operational amplifier can be used to amplify any measured small signals or difference between two signals. It can also be used to develop voltage to current/current to voltage converter. It can be utilized to develop integrator or differentiator circuits which are useful in control of electrical devices.
How AD8675ARMZ-REEL work?
![]() Figure 3 Circuit Diagram of AD8675ARMZ |
Fig.3 shows circuit diagram of AD8675ARMZ as a non-inverting operational amplifier. In this configuration, the input voltage signal, (VIN) is applied directly to the non-inverting (+) input terminal which means that the output gain of the amplifier becomes Positive. Closed loop voltage gain of a Non-inverting Operational Amplifier will be given as: . Output voltage is amplified by the voltage gain Av and can be calculated as
2-D VIEW OF AD8675ARMZ-REEL

Figure 4 2-D View of AD8675ARMZ-REEL

Figure 5 Foot-Print_AD8675ARMZ-REEL
AD8675ARMZ-REEL Related Products Prices




COMMENTS