* Question
| Hard synchronization and resynchronization are two ways of CAN synchronization. What rules do they follow? |
* Answer
| 1 Only adapt to one method in one bit time.
2 This transition edge is used for synchronization only if the value detected at the previous sampling point is different from the value after a transition edge. 3 When the bus is idle, always use hard synchronization. |

COMMENTS