• Home
  • QUESTIONS & ANSWERS
  • Programmer, development system
  • In addition to high coherence, what are the advantages of HeNe lasers?

    * Question

    In addition to high coherence, what are the advantages of HeNe lasers?


    *
    Answer

    1 easy to achieve single mode operation, and the line width is very narrow, can be as low as 1 kHz, which is more expensive for the interference type sensor;

    2 high radiation density, high coupling efficiency with single mode fiber, for example, 1 mm diameterThe circular area 氦氖 laser produces a typical output power of 1 mW with a divergence angle of approximately 1 mrad.