* Question
Method for identifying three poles of thyristor
* Answer
To identify the three terminals (poles) of a thyristor (SCR: Silicon Controlled Rectifier) — Anode (A), Cathode (K), and Gate (G) — you can use both physical observation and electrical testing methods.
Table of Contents
Toggle1. Understanding Thyristor Terminals
Anode (A): Main current input terminal.
Cathode (K): Main current output terminal.
Gate (G): Control terminal that triggers the thyristor into conduction.
2. Method for Identifying the Terminals
Method A: Visual Identification (if marking exists)
Check the package for printed labels: A, K, G.
For TO-220 packages (common for power thyristors), pinout is often:
Pin 1: Gate (G)
Pin 2: Cathode (K)
Tab/Back or Pin 3: Anode (A)
Datasheets or manufacturer documentation confirm this layout.
Method B: Multimeter Test (Diode Mode)
You can use a digital multimeter in diode mode to identify the terminals.
Step-by-step procedure:
Find the Gate and Cathode:
Place the positive probe on the Gate and the negative probe on another terminal.
If the meter shows a low forward voltage drop (~0.6V to 0.8V), the second terminal is the Cathode (K) and the first is the Gate (G).
Find the Anode:
Now place the positive probe on the suspected Anode and the negative on the Cathode.
Normally, an SCR won’t conduct unless triggered.
Temporarily short the Gate and Anode with a wire (simulate trigger), then measure again across Anode to Cathode.
If the meter now shows low resistance or conduction, then the terminals are correctly identified.
Method C: Use of Test Circuit (if multimeter is inconclusive)
Build a simple test circuit with:
A small DC power source (e.g., 9V)
A load resistor in series with the thyristor
A push-button switch from Gate to Anode
Steps:
Connect the circuit with assumed Anode and Cathode.
Press the Gate button; if the load turns on and remains on, you’ve correctly identified the Gate, Anode, and Cathode.
Summary Table
Terminal | Function | Test Method |
Gate (G) | Trigger input | Forward diode test with K |
Cathode (K) | Negative side of main current | Common to Gate in diode test |
Anode (A) | Positive side of main current | Identified via conduction when G is pulsed |

COMMENTS