* Question What are the commonly used loop statements? * Answer Commonly used loop statements are FOR and WHILE.
* Question How does the luminous intensity modulation sensor work? * Answer The illuminating intensity modulation sensor realizes the monitoring…
* Question What is the rater? * Answer Also known as “magnification Resistors.”A Resistors used to increase the meter range…
* Question What are the subroutine call, return and null operation instructions? * Answer (1) Short call instruction (2) Long…
* Question How to add comprehensive optimization parameters? * Answer In general, there are two ways to add a comprehensive…
* Question What is a semiconductor thermistor? * Answer A semiconductor thermistor is a temperature sensor fabricated from a semiconductor…
* Question What are the characteristics of logic analyzers and oscilloscopes? * Answer Logic analyzers have similarities and differences to…
* Question Which two cryptographic algorithms are commonly used in IC card systems? * Answer (1) A symmetric key cryptographic…
* Question What are the main transmission parameter parameters? * Answer The transmission characteristic parameters mainly include current transmission ratio…
* Question How to use Altera’s basic megafunctions? * Answer Customize basic macro function parameters with Altera’s IP tool MegaWizard…