* Question What are the inverter operation control functions? * Answer 1.Starting frequency 2.Adding and decelerating time 3.Jog operation 4.DC…
* Question What points should I pay attention to when using the antenna in the room system? * Answer (1)…
* Question What are the main performance characteristics of TJAl040? * Answer (1) Full compliance with IS011898; (2) High speed…
* Question What is a conductivity type chemical sensor? * Answer A conductivity type chemical sensor is a measuring device…
* Question Which types of circuits can be divided into source drive circuits depending on whether a digital-to-analog converter (DAC)…
* Question What are the advantages of the LIN system? * Answer (1) System flexibility (2) Message routing (3) Multicast…
* Question The technical parameters of the А/D converter reflect its performance characteristics. What are the main indicators? * Answer…
* Question What is the power supply design specification? * Answer (1) The full voltage input range is AC90 ~…
* Question What are the triggering methods for interrupts? * Answer There are two types of interrupt triggering methods: edge…
* Question What are the stages of the control law accelerator pipeline? * Answer Take instruction 1 (F1), fetch 2…