* Question
| What are the advantages of the CSUE communication network system over the currently approved underground mine communication system? |
* Answer
| • The CSUE network can be configured as a redundant mesh to provide ground-to-ground communication (eg, due to top collapse) even when the repeater fails or the repeater loses connectivity.
• After the power is removed, the battery backup communication relay will maintain the underground network function for hours or even days (depending on specific requirements). • With fire, collapse, explosion, etc., after detecting a faulty and failed repeater, information on the location of the emergency can be quickly provided. • The CSUE network can be programmed to provide location information for the terminal miners to the ground.The data of the miner’s approximate distance to the nearest repeater can be displayed in near real time. |

COMMENTS