* Question
| What are the aspects of embedded Flash programming? |
* Answer
| (1) Programmer Programming It is the most primitive method of programming.A special programmer is used to write code or data to the chip before the programming chip is soldered to the board, and then the programmed chip is mounted on the board.
3) JTAG programming This programming method is to directly use the device with JTAG interface on the board (such as CPU, CPLD, FPGA, etc.), and then connect the target board to the host through the JTAG emulator of the same interface, and flash on the target machine.Programming.(p. 42) |

COMMENTS