* Question
| What are the characteristics of the three stepper motors? |
* Answer
| Reactive stepping motor is generally three-phase, can achieve large torque output, the step angle is generally 1.5 °, but the noise and vibration are very large; permanent magnet stepping motor is generally two-phase, torque and volume is smallThe step angle is generally 7.5 ° or 15 °; the hybrid stepping motor combines the advantages of the permanent magnet stepping motor and the reactive stepping motor. |

COMMENTS