* Question
What are the command registers of SJAl000?
* Answer
The SJAl000 series refers to a family of Serial Communication (CAN) controllers, often used in embedded systems for communication via the Controller Area Network (CAN) protocol. The command registers are critical for controlling and configuring the operation of the controller, allowing you to initialize, manage, and monitor the CAN communication.
Below are some common command registers found in a typical SJAl000 CAN controller series (depending on the specific version, the names and bit positions might vary slightly):
Table of Contents
Toggle1. Control Register (CR)
The Control Register is the primary register for initiating commands and configuring the operation of the CAN controller. It typically includes control bits for enabling specific operational modes and performing system tasks.
CR[INIT]: Initialization Command. Writing a 1 to this bit initiates the initialization mode.
CR[LISTEN]: Listen-Only Mode. If set, the CAN controller operates in listen-only mode, meaning it does not transmit messages but can receive and listen to the CAN bus.
CR[TRANSMIT]: Start Transmission. Writing 1 initiates the transmission of data from the buffer.
CR[ABORT]: Abort Current Transmission. Writing 1 aborts any ongoing transmission and clears the transmission request.
CR[RECEIVE]: Receive Command. Enables the receiver to accept incoming data messages.
2. Status Register (SR)
The Status Register is used to monitor the current operational state of the CAN controller and to indicate various status flags.
SR[RXOK]: Receive OK Flag. Indicates whether the CAN controller has successfully received a message.
SR[TXOK]: Transmit OK Flag. Indicates whether a message has been successfully transmitted.
SR[ERR]: Error Flag. A flag that shows if an error has occurred in the CAN communication.
SR[BUSY]: Busy Flag. Shows whether the CAN controller is currently processing data (either transmitting or receiving).
SR[IDLE]: Idle Flag. Indicates if the CAN controller is idle (i.e., no ongoing communication activity).
3. Command/Status Register (C/S)
A Command/Status Register can combine both control commands and status indicators.
C/S[START]: Start Command. Initiates the CAN communication process.
C/S[STOP]: Stop Command. Stops CAN communication.
C/S[RESET]: Reset Command. Resets the CAN controller to its initial state.
4. Interrupt Enable Register (IER)
The Interrupt Enable Register is used to enable or disable the interrupt sources for the CAN controller.
IER[RXIE]: Receive Interrupt Enable. Enables an interrupt when a message is successfully received.
IER[TXIE]: Transmit Interrupt Enable. Enables an interrupt when a message is successfully transmitted.
IER[ERRIE]: Error Interrupt Enable. Enables an interrupt when an error occurs.
IER[BUSYIE]: Busy Interrupt Enable. Triggers an interrupt when the controller is busy.
5. Error Register (ER)
The Error Register is used to monitor and handle errors during CAN communication.
ER[TXERR]: Transmit Error. Indicates a transmission error (e.g., bit errors, CRC errors).
ER[RXERR]: Receive Error. Indicates a reception error (e.g., overrun, bit stuffing errors).
ER[BUSERR]: Bus Error. This flag is set if the CAN controller detects an issue with the bus state, such as an arbitration loss or error frame.
6. Transmit Buffer Register (TXB)
The Transmit Buffer Register is used to load data into the transmit buffer of the CAN controller for transmission.
TXB[DATA]: Data Field. Contains the actual data to be transmitted over the CAN bus.
TXB[ID]: Identifier Field. Holds the CAN message identifier.
7. Receive Buffer Register (RXB)
The Receive Buffer Register stores received messages from the CAN bus.
RXB[DATA]: Data Field. Holds the received data.
RXB[ID]: Identifier Field. Contains the message identifier of the received CAN message.
8. Bit Timing Register (BTR)
The Bit Timing Register configures the bit rate and synchronization of the CAN bus communication.
BTR[BRP]: Baud Rate Prescaler. Configures the baud rate of the CAN bus.
BTR[TSEG1]: Time Segment 1. Sets the length of the first time segment in bit time.
BTR[TSEG2]: Time Segment 2. Sets the length of the second time segment.
BTR[SJW]: Synchronization Jump Width. Used to adjust the synchronization between nodes to prevent errors.
9. Acceptance Mask Register (AMR)
The Acceptance Mask Register is used for filtering incoming messages based on their identifiers.
AMR[AM]: Acceptance Mask. Determines which CAN message identifiers are accepted by the controller.
AMR[EXT]: Extended Identifier Mask. Enables or disables the acceptance of extended CAN identifiers (29 bits).
10. Interrupt Status Register (ISR)
The Interrupt Status Register is used to read the current interrupt status of the CAN controller.
ISR[RXINT]: Receive Interrupt. This flag is set when a message is received.
ISR[TXINT]: Transmit Interrupt. This flag is set when a message is transmitted.
ISR[ERRINT]: Error Interrupt. This flag is set when an error occurs.
Conclusion:
The SJAl000 CAN controller series typically includes a range of command registers for controlling its operation, monitoring its status, and handling interrupts. These registers are essential for enabling features such as initialization, error handling, and communication management in CAN-based systems. The specific names and details of these registers can vary slightly depending on the manufacturer or model of the SJAl000 series, but these basic functions are common across most implementations.

COMMENTS