• Home
  • QUESTIONS & ANSWERS
  • Power Supplies - Board Mount
  • What are the main factors causing electromagnetic interference?

    * Question

    What are the main factors causing electromagnetic interference?

    * Answer

    The main factors causing electromagnetic interference (EMI) include the following:

    1. Electromagnetic Emissions: Any device that generates electrical signals can emit electromagnetic waves, which can interfere with nearby electronic equipment. Common sources include motors, power lines, and fluorescent lighting.

    2. High-Frequency Devices: Devices operating at high frequencies, such as microwaves, Wi-Fi routers, and cellular devices, can produce signals that interfere with other nearby electronic systems.

    3. Power Supply Fluctuations: Variations in power supply, especially from high-voltage equipment, can generate electrical noise and spikes that result in EMI. This is common in environments with heavy machinery or industrial equipment.

    4. Environmental Factors: Natural phenomena, like lightning or solar flares, produce electromagnetic fields that can disrupt electronic systems. Even seasonal electrical storms can be a cause of EMI in sensitive equipment.

    5. Poor Shielding and Grounding: Inadequate shielding or grounding of electronic equipment allows interference from external sources to penetrate and disrupt signals, making devices more susceptible to EMI.

    6. Proximity of Devices: Devices placed too close together, especially those with sensitive or unshielded electronics, can cause crosstalk and EMI. Dense installations in data centers or manufacturing plants often need special consideration for spacing and shielding.

    7. Switching Electronics: Power electronics with switching components, such as switching power supplies and inverters, generate high-frequency noise that contributes to EMI. The rapid switching can create electromagnetic waves that radiate into the surroundings.

    8. Electrical Wiring and Cables: Long cables, particularly those that are poorly shielded, can act as antennas, picking up EMI from surrounding equipment and electrical noise from power lines.

    9. Human-Caused Factors: Activities like welding, radio broadcasting, and even mobile phone usage near sensitive equipment can introduce EMI due to the strong signals these activities generate.

    Managing these factors is key in reducing EMI, especially in environments with highly sensitive electronic equipment. Proper shielding, grounding, spacing, and the use of filters can help mitigate these interference sources.