• Home
  • QUESTIONS & ANSWERS
  • Others
  • What are the main features of the Enhanced Capture (eCAP) module?

    * Question

    What are the main features of the Enhanced Capture (eCAP) module?


    *
    Answer

    4 event time stamped register registers; up to 4 time stamp stamp capture events can be selected for edge polarity; each of 4 events can generate an interrupt; can capture up to 4 event time stamps in a single capture;Continuous capture of time stamps in the stage loop buffer; capture of absolute time stamps; capture of differential modes