* Question
| What are the main technical features of CAT3200/3200-5? |
* Answer
| 1 fixed operating frequency is 2MHz;
2100mA output current; 3 output voltage is stable (CAT3200-5 is fixed to 5V, CAT3200 output voltage is adjustable); 4 low quiescent current (typical value of 1.7mA); 5 input voltage is as low as 2.7V still works normally; 6 has soft start, slope control function; 7 low value external capacitor (1 |

COMMENTS