* Question
| What are the main technical features of the MAX7316? |
* Answer
| 1400kbit/s, 2-wire serial interface, 5.5V voltage tolerance;
2 working voltage is 2~3.6V; 38-bit PWM white LED brightness control, global 16-level brightness control, additional l6 independent brightness control; 4 twoThe white LED flashes; 55.5V input overvoltage protection, the input clears the serial port status, |

COMMENTS