* Question
| What are the main technical features of the TPS7510x? |
* Answer
| 1 Eliminates the influence of electromagnetic interference (EMI) because it does not need internal switching signal;
2 output current matching accuracy is: 2%; 3 common cathode structure, driving up to 4 LEDs with each 25mA power; 4 in lithiumIn ion battery applications,The default LED current saves external components; 7 with the innovative factory EEPROM programming technology, the default value can be set in the range of 3 ~ 10mA (step increment is lmA); 8 with over current and overheat protection. |

COMMENTS